TGML Scaling: <Scale>

Scale scales the coordinate system for the immediate parent element.

Attribute Type Description

Center

Point

Describes the position of the center point (origin) of the scale.
For more information, see the TGML Rotation: <Rotate> section.
Default: "0.5 , 0.5"
Inheritable: No
Animatable: Yes

ScaleX

Double

The horizontal scale factor.
Default: "0.0"
Inheritable: No
Animatable: Yes

ScaleY

Double

The vertical scale factor.
Default: "0.0"
Inheritable: No
Animatable: Yes